• Land/Region
  •   
 
Resource Page / Anwendungshinweise / Testen und Messen / Gauging Depth of Field in Your Imaging System
Gauging Depth of Field in Your Imaging System
Edmund Optics Inc.

Gauging Depth of Field in Your Imaging System

Gauging Depth of Field in Your Imaging System

Over the years, we have answered countless questions regarding lens performance. Of those questions, none have been more difficult to define than requests for depth of field. The reason for this difficulty has more to do with the vagueness of the question than with the inability to provide a measured or calculated value. Consider for a moment what depth of field tells us. It is the distance by which an object may be shifted before an unacceptable blur is produced. For depth of field to be properly stated, it should contain not only the displacement of an image, but also a specific resolution. The depth of field specification is further complicated by a type of keystoning aberration that often occurs. This result can dramatically affect linear measurements and therefore render depth of field unusable. In this article we will take a closer look at depth of field calculations and compare them to physical measurements using the DOF 1-40 depth of field gauge. The gauge, as we will see later, offers a unique look at what depth of field really means and how we as system designers may wish to quantify this parameter. A simple geometric approximation for depth of field is shown in Figure 1.0. The linear blur (required resolution) Bp, Bm and Bf can be expressed in terms of angular blur by the following equation.

Figure 1
Figure 1

Using similar triangles, a relationship can now be made between angular blur and the focus point,

(1)$$ \omega = \frac{B_f}{D} = \frac{B_p}{D + \delta_{+}} = \frac{B_m}{D - \delta_{-}} $$
(2)$$ \frac{A}{D} = \omega \cdot \left( \frac{D + \delta_{+}}{\delta_{+}} \right) = \omega \cdot \left( \frac{D - \delta_{-}}{\delta_{-}} \right) $$

where λ is the aperture of the lens. Solving for δ+ and δ,

(3)\begin{align} \delta_{+} & = \frac{\omega \cdot D^2 }{\left( A + \omega \cdot D \right)} \\ \delta_{-} & = \frac{\omega \cdot D^2 }{\left( A - \omega \cdot D \right)} \end{align}

The derivation above is very specific to the intended resolution. However, many theoretical derivations of depth of field often assume the lens resolution to be nearly diffraction limited. The most popular of these derivations are based on microscope applications. A typical example for the total depth of field (δ+ + δ) is shown below.

(4)$$ \text{Delta Theory} = \left( \delta_{+} + \delta_{-} \right) = \frac{\lambda}{\left( \text{NA} \right) ^2}$$

Where λ is the wavelength and NA equals the numerical aperture of the lens.

In order to study depth of field we have put together a simple macro system consisting of a 25mm fixed focal length lens, 8mm spacer and Sony XC-75 monochrome CCD video camera. The system was chosen not for its performance but rather for its common real world implementation. Measurements were performed using the DOF 1-40 target. The target allows us to measure depth of field at either 1, 10, 20 or 40 lp/mm over a maximum depth of 50mm. The flat field resolution of this system is approximately 15 lp/mm at 0.3X primary magnification. For purposes of our experiment, a blur spot resolution of 0.1 mm or 10 lp/mm was chosen. Depth of field measurements were taken at three aperture settings corresponding to f/2, f/4, and f/8. An important point should be noted about aperture settings. The f-number shown on most fixed focal length lenses is calculated with the object at infinity. As a result, we have adjusted our NA and therefore our aperture values for a 95mm working distance.

The values below highlight a number of points to consider. In general our calculated and measured delta d are fairly close. However, the displacement of the image due to defocus aberrations was not predicted by our calculations. This type of displacement error could certainly be problematic if the system contained an auto iris. If we compare our measured results to the delta-theory, we notice a significant variation. As we mentioned earlier, this variation is due to a false assumption concerning system resolution.

Another property that should be noted in our DOF 1-40 observations is the non-uniform magnification seen through the depth of field range. This is a very common problem in most lenses and, as we stated earlier, can yield significant errors if measurements are made throughout the full depth of field range. Edmund Optics provides several telecentric options to correct for this type of error.

In the end, it is the total performance of an optical system that counts. As a full service supplier and manufacturer of optics, illumination, CCD cameras, monitors, mounting, and electronic imaging related products, Edmund Optics has the knowledge and resources to look at your application as a total system. In fact, innovative tools such as the DOF 1-40 have come about from our own in-house need to quantify system performance. So if you are looking for individual components that can be integrated into your system or starting from scratch, our engineers are ready to help.

Table

References

  1. Smith, Warren J. Modern Optical Engineering. 2nd ed. New York, NY: McGraw-Hill Education, 1990.
War dieser Inhalt nützlich für Sie?

Testcharts werden zur Evaluation oder Kalibrierung der Leistung eines Bildaufnahmesystems verwendet. Wir helfen Ihnen dabei, das richtige Testchart für Ihre Anwendung auszuwählen.

Testing resolution or distortion? Measuring image quality or color or grayscale performance? Check out our selection of test targets on glass, chrome, or photographic paper.

Erfahren Sie wie Schärfentiefe und Auflösung miteinander verbunden sind und wie Faktoren wie bspw. die Blende ein Bildverarbeitungssystem beeinflussen.

Edmund Optics can not only help you learn how to specify the right imaging optics, but can also provide you with multiple resources and products to surpass your imaging needs.

Sie haben Fragen? Nehmen Sie Kontakt mit uns auf!

Angebot erwünscht? Bitte geben Sie eine Artikelnummer ein.

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram



EO IST MITGLIED VON:

Spectaris Optence Photonics21 Epic EMVA EOS Photonics France

×