Bildgebungselektronik 101: Kameraauflösung und ihr Einfluss auf die Bildqualität
Die Kameraauflösung und der Kontrast spielen eine wichtige Rolle, sowohl für die Optik als auch die Elektronik eines Bildgebungssystems. Mehr erfahren!
I recently removed an optical low pass filter from my digital camera. Do you have any suggestions on how to measure its Modulation Transfer Function (MTF)?
I recently removed the IR cut filter from my camera and did not replace it with any type of clear glass. It has since lost sensitivity in the IR, which was the goal, but also focus ability in the optics. Can you explain why this is so?
Are you new to imaging and want to learn more about lens magnification? Learn more about lens magnification and other key imaging concepts at Edmund Optics.
Verwenden Sie häufig Bildverarbeitungssysteme in Ihrem Beruf? Bei Edmund Optics finden Sie Tipps und Praktiken für verbesserte Bildverarbeitungssysteme.
LIGHT TALK - EPISODE 1: Machine Vision Trends with Nick Sischka
Join our discussion around machine vision trends including such as increasing resolution and new sensors in the first episode of our LIGHT TALKS series.
Learn how Edmund Optics maintains optical performance across the entire image plane through this resolution and contrast comparison using our C Series FFL lens.
I have two Basler Scout GigE cameras but I cannot use them simultaneously. When connected to a computer, either via two network cards or a single network card and a switch, they can be opened but cannot acquire images. What is causing the problem?
I am looking for a way to power a camera and a 3.3V, 2W laser (always on) in an OEM application. Which of the two - USB or Firewire – can sustain more power?