Produkt in den Warenkorb gelegt
Danfoss logo

Case Study:
How Danfoss IXA and Edmund Optics are creating a Cleaner Environment

The Future Depends on Monitoring and Regulating Air Pollution, Which is an Essential Step Towards Creating a Cleaner Environment

Monitoring Maritime
Pollution with Optics

Monitoring and regulating air pollution is an essential step towards creating a cleaner environment. Danfoss IXA, a high-tech company based in Denmark, is developing a device called MES 1001, a marine emission sensor based on ultraviolet absorption spectroscopy which monitors the NO, NO2, SO2 and NH3 emissions produced by cargo ships to ensure that they are complying with all environmental regulations. The optical sensor is placed inside the exhaust system of ships, so the involved optics will be exposed to extreme conditions and must be able to withstand temperatures up to 500°C and very high pressures simultaneously.

Danfoss IXA was looking for a partner to develop optics fulfilling their demanding requirements, and in Edmund Optics® (EO) they found a partner who was prepared to take on this challenge which went beyond their normal capabilities. Edmund Optics created custom test beds for verifying the unique requirements of the sensor, which enabled Edmund Optics to develop a robust system to meet Danfoss IXA’s specifications.

Danfoss IXA develops sensors and systems for the maritime industry, focusing on energy optimization and the measurement of emission gases. They are a part of the Danfoss Group, a global enterprise which produces a wide range of technologies that address a variety of markets including food supply, energy efficiency, and climate-friendly solutions.  

Smokestack emissions from international shipping are a severe problem for human health, contributing to the premature mortality of people all across the world from lung damage and cardio vascular diseases.

Creating a Cleaner
Environment Starts At Sea

The International Maritime Organization (IMO) has recently decided that commercial ships must comply with low sulfur fuel requirements globally by 2020. In addition, the current Nitrogen Oxide emission control area along the North American coastline will be expanded to cover the Baltic and North Seas in 2021. There currently aren’t convenient and reliable ways for the IMO to monitor ships’ emissions and enforce these regulations. A multitude of local and regional initiatives seeking to limit the air emission from ships further underline the fact that the industry needs to adapt to a world where strict emission requirements are part of the game. Danfoss IXA is developing the MES1001, which is a comprehensive marine emissions sensor suitable for accurately measuring a ship’s air emissions in real time.  

NO2 and SO2 emissions from international shipping around Europe are expected to surpass the total from all land-based sources in the 28 EU member states combined by 2020 or 2025
Figure 1: "NO2 and SO2 emissions from international shipping around Europe are expected to surpass the total from all land-based sources in the 28 EU member states combined by 2020 or 2025"

The Challenge

Danfoss IXA approached several providers of optical components to jointly design the optical system for the new MES 1001 device. This project turned out to be very challenging due to the extreme high temperature and pressure requirements. High temperatures can cause optics to fail due to melting and thermal stresses, which severely limits the types of optical materials that can be used. High temperatures can also cause adhesives used in the optical assembly to outgas, contaminating the system. The high pressure requirements made the sealing of the optical system critically important. Most of the optics partners faced their limits in terms of design, metrology for these harsh conditions, or working across different continents and time zones.  

The Solution

Edmund Optics® (EO), with its global presence and large staff of optical engineers and designers, is always keen to face new challenges. One of the reasons that Danfoss IXA selected Edmund Optics as a partner is their ability to ramp-up products from prototype to volume production. When approached by Danfoss, Edmund Optics dedicated R&D and project management resources to developing an optical assembly for the MES 1001, even though Edmund Optics had never designed systems to work at temperatures as high as 500°C before. Edmund Optics investigated many different materials and mounting options, recognizing this project as a learning experience and opportunity to expand their capabilities. Custom testbeds for verifying the optical system’s unique requirements were created and proper sealants and optomechanics were identified to allow the assembly to survive these high pressures. The start of that development process was faced with many issues including cracking optics and outgassing adhesives, but by iterating the design process multiple times and researching in different materials these issues were solved and Edmund Optics eventually delivered an optical assembly that could survive the harsh environment inside a ship’s exhaust system. Edmund Optics is proud to be a part of this product which will positively impact the environment and support a global effort to reduce harmful emissions.

Danfoss IXA “greatly appreciated Edmund Optics’ professional way of involving [them] along the development process as well as their ability to adapt to changing requirements as [Danfoss IXA] learned more about the exact conditions in which the sensor would be used.” During that time Danfoss IXA “found the support from Edmund Optics’ project managers extremely fruitful and very efficient in bringing the development process to success.”

The robust optical system is a critical component of the new MES 1001 device, which was launched in 2017. It was exciting for Edmund Optics to work on this cutting-edge technology in such a close collaboration with Danfoss IXA’s skilled research and development team. The MES 1001 will allow the IMO and other organizations to enforce maritime emissions requirements and help lead to a cleaner environment across the globe.  

During that time Danfoss IXA

“found the support from [Edmund Optics'] project managers extremely fruitful and very efficient in bringing the development process to success.”

- Finn Haugaard, Danfoss IXA

War dieser Inhalt nützlich für Sie?
The Future Depends on Optics
 
Vertrieb & Beratung
 
weitere regionale Telefonnummern
Einfaches
ANGEBOTSTOOL
Geben Sie zum Starten die Produktnummer ein.
;